Apply to be a TradeMaster!
Main product image of Magnecover Adjustable Magnetic Umbrella Kit
Magnifying glass
Hover image to zoom

Magnecover Adjustable Magnetic Umbrella Kit

Brand:
Supco
SKU:
MUKIT
Rating:
(79)
Q&A:
(0)
Magnecover Adjustable Magnetic Umbrella Kit
Magnifying glass
Hover image to zoom
$70.18 each
In Stock
In Stock
Get 49 Tue, Nov 24
Order by today, receive Tuesday
Free Shipping On orders over $99
Easy Returns No restocking fee for 90 days

Product Highlights

–
Product Highlight: Height (Inches)
38" Height
Product Highlight: Width (Inches)
60" Width

Description

–
The SUPCO TradeFox Magnetic Umbrella has taken the HVAC industry by storm, and techs can't seem to work without it. It keeps them protected on scorching rooftops, and dry during rainy repairs.

Features:
  • 60" wide
  • Waterproof, UV-coated umbrella with durable and flexible fiberglass ribs
  • Patented base swivels and locks
  • Heavy-duty magnet attaches securely to any metal housing

Kit includes:
  • New SUPCO TRADEFOX Lanyard (MULNYD)
  • Umbrella (MUUMB)
  • Magnetic Base (MUBASE)

Specs

–
Product Type:

Umbrella

Height (Inches):

38"

Width (Inches):

60"

Help Face

Questions?

Speak with a real person who will go out of the way to help!
Call or text 888-757-4774
Monday – Thursday
8am–7:45pm
Friday
9am–7:45pm
Saturday – Sunday
9am–5:45pm


You May Also Need

Extension Pole for Magnetic Umbrella
SKU: MUPOLE
Supco

Product Reviews

4.34 out of 79 reviews
83% would recommend this product
4.34
out of 79 Reviews
83% would recommend this product
WRITE A REVIEW
5 star
73%
4 star
9%
3 star
5%
2 star
4%
1 star
9%
WRITE A REVIEW
Customer Images

Most Liked Positive Review

Magnet not that strong

The umbrella is great! Works well, easy to carry and gives me shade on roofs. Just beware, the magnet is nowhere near as strong as advertised. While it does keep the umbrella hanging upside-down in my van, it does not hold my gauges or tool bag. It also blew off the roof with a light breeze and broke two of the arms.
VS

Most Liked Negative Review

Not the quality that I was expecting.

I was very excited when I purchased this item. I am a commercial HVAC technician in Miami and I spend a lot of time on rooftops in the sun. This umbrella seemed like the perfect product and I have been using it for the last few weeks since I purchased it. However, the quality is less than I was expecting. After just a few weeks one of the spokes has already snapped from some very reasonable use and the metal sleeve that goes over where the umbrella goes into the magnet is already falling off, the glue appears to have given out. For the price, I expected something a bit more durable, especially since the product is geared towards technicians working in the field. I will continue to use it for as long as it lasts, since have shade when working on rooftops is invaluable and the product most certainly provides it.
Showing 1-10 of 79 reviews

Awesome for HVAC Tech

I bought this for my son because he's an HVAC Technician, and with how hot it is in the summer in Texas, he said that this is really helping make a difference when he has to be out on the roofs. He said it's sturdy, a wide protection from the umbrella, and keeps the heat from beating down on him. He highly recommends it.
MomofHVACTech
Temple, TX
4 months ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

broke in first week

i have been through many kinds but like the rest these things just not made to last, they should be considered a one time use
Mike
South Louisiana
4 months ago
Was this review helpful to you?

Exactly what I needed

Used during some heavy rains in order to stay "dry" and work under unfavorable conditions. Often used when its hot to provide some shade - with the metal base it sticks almost anywhere and is very moveable
Supplyguy
Massachusetts
6 months ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

So far so good

Seems heavy duty
Goldie Loc
Los Angeles
1 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

I would buy this again

Easy to assemble. The clamping holds hold well but time will tell. The CON is this is not designed to be used in windy environments.
edwoo
Brentwood, CA
1 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Umbrella great quality works well

Umbrella works well keeps keeps you working in the shade
Gary
New York and New Jersey
1 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Never

Base is quality The actual umbrella very cheap broke 4th time I used it This is criminal and robbery
Hek tek
New York
1 years ago
Was this review helpful to you?

Keeping cool in the hot sun

It's 110 in Las Vegas it's a necessary to have while working out here
Chris right
Las Vegas
1 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

i would buy this product again

service techs love them!
jim
lakewood
2 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Works great, but broke within the first 5 uses

It's awesome magnet is super strong, but one of the little arms that opens the canopy broke the second or third time I used it. Still functions.
Lucious
Houlton maine
2 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?
Free Shipping
On orders over $99
We offer flexible shipping and scheduling options, up-to-date delivery estimates, and free ground shipping on any order over $99 to make sure your order gets to you on-time, for less.
Shipping Policy
Easy Returns
Returning items is as simple as 1-2-3
Ordered the wrong product? Item damaged in transit? Our 3-step process makes returning products easy – even up to a year after purchase – with no restocking fees on returns made within 90 days.
Return Policy