Shop Resideo Sale
Main product image of Jumper King, Multi-Jumper with Selector
Magnifying glass
Hover image to zoom
Jumper King, Multi-Jumper with Selector
Magnifying glass
Hover image to zoom
$79.71 each
In Stock
In Stock
Get 25 Tue, Nov 17
Order by today, receive Tuesday
Free Shipping On orders over $99
Easy Returns No restocking fee for 90 days

Product Highlights

–
Product Highlight: Length
20"
Product Highlight: Voltage
24 VAC

Description

–
The Jumper King allows you to quickly bypass any low voltage thermostat regardless of terminal style. This patent-pending all-in-one kit comes with everything you need to locate low-voltage shorts and eliminate compressor short cycling.

Specifications
  • For Use on low voltage circuits only (0-30VAC/VDC).
  • 6-Alligator Clips, 6-Magnetic Tips, 6-Jumper Leads, 6-Self Piercing Insulation Tips.
  • Spade Adapters, Jumper King Thermostat Bypass Tool, Hard Carrying Case.
  • Will never short out - contains a resettable popper fuse.
  • Innovative selector switches to activate leads/circuits of your choosing at any time
  • Rugged unit has a rubberized boot, a magnet and fold-out hook for convenient mounting.
  • Four types of interchangeable tips: spade adapters, alligator clamps, magnetic tips and self-piercing insulation tips.
  • No batteries required - powered by the low voltage in the A/C unit.
  • Works on multiple stage units including heat pumps.

Specs

–
Product Type:

Jumper

Length:

20"

Voltage:

24 VAC

Help Face

Questions?

Speak with a real person who will go out of the way to help!
Call or text 888-757-4774
Monday – Thursday
8am–7:45pm
Friday
9am–7:45pm
Saturday – Sunday
9am–5:45pm


You May Also Need

Product Reviews

4.83 out of 24 reviews
100% would recommend this product
4.83
out of 24 Reviews
100% would recommend this product
WRITE A REVIEW
5 star
88%
4 star
8%
3 star
4%
2 star
0%
1 star
0%
WRITE A REVIEW
Customer Images

Most Liked Positive Review

Great, Not So Little, Tester

Product works well. Has every imaginable adapter combination. Comes in a nice sturdy case with elastic holders for all the adapters. Still has room for your personal jumpers and/or some wire. The over all size is bigger then expected, definitely not a pocket tool. Like the built in circuit breaker, allows for tracing issues on equipment with 3 amp blown fuses.
VS

Most Liked Negative Review

Useful, but questionable quality control

The good: This is an extremely useful tool to bypass the thermostat and safely test all low voltage functions on HVAC appliances. Its has every tool you could need to tap into control wiring, and it has enough extra space in its zipup tool pouch that you can carry lots of minutia you may want to carry along, such as 3a and 5a fuses for the RTU control board you may find has been blown once you get on the roof thereby saving you a trip back to your truck, tips and probes for your multimeter, and other such electrical accessories. Overall it has been very useful for troubleshooting and even for just regular preventative maintenance operations checks. It is worth the space it takes up over a regular jumper wire. The bad: Quality control is lacking on this product. During my first month using it, bare wire slipped out of the plugged portion on one of my jumper leads. It took some time to figure out what went wrong, but basically behind the insulated rubber covering on the prong, the wire uses a simple flathead nut to secure the wire to the prong, and apparently this prong's nut was loose. I appreciate that this results in something that is field serviceable (it is difficult, but using a regular control screwdriver I was able to take off the rubber covering, access the nut, and tighten it up enough to hold the wire again), but this is poor engineering in my opinion. I am going to have to check and tighten all the prongs on this device myself, and make it a habit to give a tug test to each individual wire each time I make use of it, and frankly I don't feel like I should have to do this. When I purchase a dedicated tool that does exactly one thing, I expect it to do it very well. Wires straight up tugging loose after such light usage bodes ill for the long term quality of this device, and as such I can only give a hesitant recommendation for other HVAC/R service technicians. Were it easier to access and tighten the screws that secure the wires, I'd rate it higher.
Showing 1-10 of 24 reviews

Good quality product

Good quality product. Works as it should. Would purchase again.
Purchasing
Hammondsport
5 months ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

This is the BEST for Rooftop/thermostat bypass!

This product is priced well and easily one of my favorite tools for my rooftop bag. Helps me diagnose the system faster, troubleshoot issues, verify items without having to jump wires loosely.
Mike
Wentzville, MO
8 months ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Must have for low voltage shorts

Favorite time saving tool.
rusty
charlotte, nc
11 months ago
Was this review helpful to you?

I Would Recommend This Tool, But

The Tool Itself Works Great, The Inline Fuse Has Saved Me Many Fuses. Carrying Case Though Is Terrible And Will Rip.
Caleb
Pa
2 years ago
Was this review helpful to you?

I Would Recommend This Tool, But

The Tool Itself Works Great, The Inline Fuse Has Saved Me Many Fuses. Carrying Case Though Is Terrible And Will Rip.
Caleb
Pa
2 years ago
Was this review helpful to you?

Love it

Very useful for troubleshooting, testing, and preventative maintenance work when used properly.
Matthew
Houston, Tx
2 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

One of my Favorite tools Ever

The jumperking has become one of my favorite, Most Regularly Used tools in my arsenal. It's part of my everyday carry. Had an issue with the reset pop-up switch not re-setting, I emailed Supplyhouse.com about it, they swapped it out with a brand new one with no hesitation. Couldn't ask for a better tool, or a better company to order it from!
Tony
South Jersey
2 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Cool tool

I like the variety of jumpers for just about any situation. Nice tool
Bill
Hedgesville wv
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Saves me everytime

I use it for troubleshooting, everyday jumping, and finding shorts. I can locate shorts in a fraction of the time with it. it's been in my daily service bag for about 8 months
Richielenz
NY
3 years ago
Was this review helpful to you?

Great price

I used this the next day after receiving it and worked great and verified the stat was faulty.
Spoony
Wichita Falls, TX
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?
Free Shipping
On orders over $99
We offer flexible shipping and scheduling options, up-to-date delivery estimates, and free ground shipping on any order over $99 to make sure your order gets to you on-time, for less.
Shipping Policy
Easy Returns
Returning items is as simple as 1-2-3
Ordered the wrong product? Item damaged in transit? Our 3-step process makes returning products easy – even up to a year after purchase – with no restocking fees on returns made within 90 days.
Return Policy