Transducers Direct was founded in 1999 to manufacture pressure transducers, pressure sensors, and pressure switches, with its headquarters in Ohio. The company builds its product line around configurable pressure sensing components rather than a fixed catalog of standard models.
Transducers Direct's engineering team supports applications across HVAC, refrigeration, and general industrial equipment, offering more than 8 million configuration options across its transducer and sensor lines.
Product Lines
The company's core lines include standard and high performance pressure transducers, wireless pressure transducers, pressure switches, and melt pressure transducers used in processing equipment.
Configurations run into the millions across these lines. Transducers Direct builds pressure sensing components to a buyer's specific pressure range, output signal, and connection type. It does not offer only a small set of fixed part numbers.
Why Contractors Specify Transducers Direct
HVAC and refrigeration technicians specify Transducers Direct pressure transducers for systems that need a specific pressure range and electrical output. These sensors are matched to the application rather than being generic off the shelf parts.
The wireless pressure transducer line also lets technicians monitor system pressure without running a signal wire back to a controller. This is useful on retrofit jobs where pulling new wire is not practical.
How to Choose Transducers Direct Products
Choosing a Transducers Direct pressure transducer starts with the system's pressure range and the output signal the control system expects. The company's configurable lineup is built around matching those two specs first.
For jobs where running a wired connection back to a controller is difficult, consider the wireless pressure transducer line in place of a standard wired unit. This works only if the monitoring location has adequate wireless range.
Frequently Asked Questions
When was Transducers Direct founded?
Transducers Direct was founded in 1999.
Where is Transducers Direct based?
Transducers Direct is headquartered in Ohio.
Does Transducers Direct make wireless pressure sensors?
Yes. Transducers Direct's product line includes wireless pressure transducers in addition to standard wired models.
How many configurations does Transducers Direct offer?
Transducers Direct offers more than 8 million configuration options across its transducer and sensor lines.
What industries use Transducers Direct products?
Transducers Direct's pressure transducers and sensors are used in HVAC, refrigeration, and general industrial applications.