Apply to be a TradeMaster!
Main product image of PEX Tube Uncoiler
Magnifying glass
Hover image to zoom

PEX Tube Uncoiler

Brand:
Bluefin
SKU:
PXTBUC
Rating:
(7)
Q&A:
(3)
PEX Tube Uncoiler
Magnifying glass
Hover image to zoom
$319.86 each
In Stock
In Stock
Get 28 Tue, Nov 3
Order by today, receive Tuesday
Free Shipping This item ships free
Easy Returns No restocking fee for 90 days

Product Highlights

–
Product Highlight: Material
Metal
Product Highlight: Tubing Compatibility
PEX-AL-PEX, PEX
Product Highlight: Warranty
2 Year Warranty

Description

–
The Tube Uncoiler facilitates the uncoiling of 5/16" to 1" PEX tubing. Simplifies installation and reduces labor. Weighted arms hold tubing in place while uncoiling. Eyelet keeps tubing from tangling. Base is collapsible. No additional hardware necessary for attaching arms. Easy to assemble.
Note: Upon assembly, the guide pin must be installed on the swivel arm in order to keep the arm in place.

Specs

–
Material:

Metal

Tubing Compatibility:

PEX-AL-PEX

PEX

Application:

5/16" PEX

3/8" PEX

1/2" PEX

5/8" PEX

3/4" PEX

1" PEX

1/2" PEX-AL-PEX

5/8" PEX-AL-PEX

3/4" PEX-AL-PEX

Type:

Tool

Warranty:

2 Year

Help Face

Questions?

Speak with a real person who will go out of the way to help!
Call or text 888-757-4774
Monday – Thursday
8am–7:45pm
Friday
9am–7:45pm
Saturday – Sunday
9am–5:45pm


Compare Similar Products

Brand
Application
Type
CURRENT ITEM
Product Image of PEX Tube Uncoiler
PEX Tube Uncoiler
SKU: PXTBUC
(7)
5/16" PEX
3/8" PEX
1/2" PEX
5/8" PEX
3/4" PEX
1" PEX
1/2" PEX-AL-PEX
5/8" PEX-AL-PEX
3/4" PEX-AL-PEX
Tool
5/16" PEX
3/8" PEX
1/2" PEX
5/8" PEX
3/4" PEX
1" PEX
1/2" PEX-AL-PEX
5/8" PEX-AL-PEX
3/4" PEX-AL-PEX
Tool
PEX Tube Uncoiler
SKU: E6061000
5/16" PEX
3/8" PEX
1/2" PEX
5/8" PEX
3/4" PEX
1" PEX
1/2" PEX-AL-PEX
5/8" PEX-AL-PEX
3/4" PEX-AL-PEX
Tool

You May Also Need

Foamboard Stapler
SKU: FBSN
Malco

Product Reviews

4.71 out of 7 reviews
100% would recommend this product
4.71
out of 7 Reviews
100% would recommend this product
WRITE A REVIEW
5 star
71%
4 star
29%
3 star
0%
2 star
0%
1 star
0%
WRITE A REVIEW
Customer Images
Showing 1-7 of 7 reviews

yes

Made the job very easy .
Mr. X
Illinois
9 months ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

This product works great.

I use this product when I run lots of upnonor or pex pipes.
Snap Ipad
Macon, ms
2 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Wow!

Great uncoiler! I was skeptical about purchasing this , but decided to give it a try.I am sure glad I did! Thing is easy to assemble after the first time and the instructions made right in the case instead of just a piece of paper is genius.There is plenty of room for a 1200 ft coil of 1/2 in but I used it with 300 ft coils which can be a problem.It was very smooth and did not fetch up or tangle once.We did not have to mount it on a board or weight it down....it just did it's job. The case is a bonus and will keep it nice foe many years.I am very impressed and highly recommend this tool. 5 stars!
Mr onetwo
Belfast, ME
2 years ago
Was this review helpful to you?

Great product

It does exactly what they describe great product make work a lot easier even though single person can do the work
Jacob
Northern Virginia
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

best investment

Huge remodel job in a crawlspace and was able to set the uncoiled outside and pull the pipe around in the crawlspace.
Antonio
Oklahoma
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Works as described

Only used it with a 300' coil so far. Easy to assemble, parts fit great in the case although something to hold the thumb screws would be a nice addition (currently using a zip lock) You must remove the thumb screws to store in the case, no big deal, simple and quick. Base is nice and wide making it stable, coil came off nicely. I didn't need to screw it into the floor.
Bob
NJ
5 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Works perfectly. Would definately recommend this product.

Workes perfectly. Would recommend this product to anybody running PEX for radiant heat. Does the job well.
Mark
Alburtis, Pennsylvania
5 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Product Q&A

3 Questions
3 Questions
ASK A QUESTION

Q: Will this work efficiently and properly with a 1000' cool of the bluefin pex tubing or is it only good for the 300'

Asked by John 3 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- SupplyHouse Staff

Hi John, thanks for writing in. Yes, this will work with a 1000' coil of PEX tubing.

Was this review helpful to you?

Q: Will this work with a 300' roll of 1" polyethylene?

Asked by Colin 3 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- SupplyHouse Staff

Hi Colin. This can be used with PEX (cross-linked polyethylene) or PEX-AL-PEX (PEX with an aluminum layer) tubing.

Was this review helpful to you?

Q: Could this also be used with poly-pipe in the irrigation industry?

Asked by John 3 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- SupplyHouse Staff

Hi John. This is specifically for use with PEX tubing.

Was this review helpful to you?
Free Shipping
On orders over $99
We offer flexible shipping and scheduling options, up-to-date delivery estimates, and free ground shipping on any order over $99 to make sure your order gets to you on-time, for less.
Shipping Policy
Easy Returns
Returning items is as simple as 1-2-3
Ordered the wrong product? Item damaged in transit? Our 3-step process makes returning products easy – even up to a year after purchase – with no restocking fees on returns made within 90 days.
Return Policy