Apply to be a TradeMaster!
Main product image of HVAC Refrigerant Copper Press Tool
Magnifying glass
Hover image to zoom

HVAC Refrigerant Copper Press Tool

Brand:
Bluefin
SKU:
ZLTLKIT
Rating:
(7)
Q&A:
(3)
HVAC Refrigerant Copper Press Tool
Magnifying glass
Hover image to zoom
$231.99 each
In Stock
In Stock
Get 81 Tomorrow, Nov 17
Order by 6PM, receive Tomorrow
Free Shipping This item ships free
Easy Returns No restocking fee for 90 days

Description

–

Note: This product is designed exclusively for 1st generation Copper Press Refrigerant fittings and is not compatible with Zoomlock MAX fittings.

Press tool kit for Copper Press Refrigerant and HVAC Fittings


Product Features

  • Includes: 1/4" 5/16" 3/8" 1/2" 5/8" 3/4" 7/8" forged jaws
  • Compact design with 360° jaw rotation

Specs

–
Product Type:

Tool Kit

Jaw Size:

1/4"

5/16"

3/8"

1/2"

5/8"

3/4"

7/8"

Help Face

Questions?

Speak with a real person who will go out of the way to help!
Call or text 888-757-4774
Monday – Thursday
8am–7:45pm
Friday
9am–7:45pm
Saturday – Sunday
9am–5:45pm

Response by Wed

Compare Similar Products

Brand
Product Type
CURRENT ITEM
Product Image of HVAC Refrigerant Copper Press Tool
HVAC Refrigerant Copper Press Tool
SKU: ZLTLKIT
(7)
Tool Kit

You May Also Need

3/8" Refrigerant Copper Press Long Radius 90° Elbow, 3031060600111
SKU: RPE038
RLS

Product Reviews

4.86 out of 7 reviews
100% would recommend this product
4.86
out of 7 Reviews
100% would recommend this product
WRITE A REVIEW
5 star
86%
4 star
14%
3 star
0%
2 star
0%
1 star
0%
WRITE A REVIEW
Showing 1-7 of 7 reviews

bailedout ,Fire permit not needed for install.

Quality Tool !
Shemp
philadelphia
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Yes if I needed

Nice tool ,used for a month now in my daily installations
Baros presicion
Tampa florida
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Works great so far.

This tool worked good on 3/8 and 3/4 couplers for a split residential system. Some fittings needed to be pressed before placing the equipment.
Ike
Utah
4 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

I definitely would buy this tool again.

I bought this press because I wanted to be able to use the press fittings when needed but was not Interested in spending thousands of dollars on a battery powered press kit that I knew I wouldn't use much. I have only used this tool on test pieces but I feel it works very well. I was even able to use on a Zoomlock plus fitting, but needed to crimp it twice for a good connection. The tool is rather bulky and heavy but it does work well. I wish there was a hand hydraulic tool that could take the different jaws, but I am very happy with this tool. The price was excellent also. I do recommend this tool
John S
Jupiter, Florida
4 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Totally On Board Now

At first I was doubtful about these types of fittings but after using them myself I gotta say wow. Super impressed with the ease of use and adaptability of the tool.
AL
FL
4 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Awesome price

Worked great on zoomlock fittings. If trying to get in very close area,, the Jaws are too big. But for my hvac project I had plenty of room. Great too if you can't afford the expensive ones 👍👍👍
DIY guy
Pa
6 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Definitely a useful tool

Excellent product! Works great and has all size heads from 1/4 all the way to 7/8. It does require more space then a motorized tool of course so that should be considered.
James
Oregon
7 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Product Q&A

3 Questions
3 Questions
ASK A QUESTION

Q: are replacement jaws available

Asked by chris 3 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- SupplyHouse Staff

Hi Chris, thanks for writing in. Unfortunately, the jaws are not available separately and so in order to replace them you would need to purchase the entire tool kit.

Was this review helpful to you?

Q: Does it come calibrated and how do you know when it needs to be calibrated again?

Asked by Ethan 3 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- SupplyHouse

Hi Ethan! There is no calibration necessary, it is calibrated at the factory.

Was this review helpful to you?

Q: Is this tool compatible with the fittings that you sell at: https://www.supplyhouse.com/ZoomLock-Refrigerant-Fittings-28344000

Asked by vacorda 5 years ago

Add your answer

* Required Field
Verified Author and ReplyVerified Reply- SupplyHouse

Hi Vacorda! The compatible fittings we carry for this tool are as follows. The RLS Fittings which can be found on our website here: https://www.supplyhouse.com/RLS-Refrigerant-Fittings-30260000 and the ZoomLock 1st generation fittings which can be found on our website here: https://www.supplyhouse.com/ZoomLock-Refrigerant-Fittings-28344000 Please note this tool is NOT compatible with the ZoomLock MAX fittings.

Was this review helpful to you?
Free Shipping
On orders over $99
We offer flexible shipping and scheduling options, up-to-date delivery estimates, and free ground shipping on any order over $99 to make sure your order gets to you on-time, for less.
Shipping Policy
Easy Returns
Returning items is as simple as 1-2-3
Ordered the wrong product? Item damaged in transit? Our 3-step process makes returning products easy – even up to a year after purchase – with no restocking fees on returns made within 90 days.
Return Policy