Champion Irrigation Products started in 1937 in Los Angeles, California, building sprinkler heads and valves for the growing irrigation trade in Southern California. The company has since relocated its headquarters to Memphis, Tennessee, while keeping the same focus on brass and durable-material components for lawn and landscape irrigation systems. Champion's customer base spans contractors, wholesalers, retailers, and homeowners, with installations found on golf courses, agricultural fields, parking lots, and community landscapes across the country. Nearly nine decades in the irrigation business have shaped a product line built around straightforward repair and replacement parts that installers can source without redesigning an existing system.
Product Lines
Champion's irrigation valve line includes anti-siphon valves, automatic anti-siphon valves, manual valves, inline valves, ball valves, hose bibs, sillcocks, and vacuum breakers. These cover both new installations and valve-box replacements. The sprinkler and sprinkler-parts line covers impulse sprinklers, rotor sprinklers, retractable sprinklers, spray pop-up bodies, and pressure-regulated sprinklers. It also includes nozzles sized for different spray patterns and coverage areas. Fittings and connections round out the core catalog with brass fittings and automatic actuators for valve control. Champion also makes gas log lighter valves and log lighter bars, a specialty line that overlaps with fireplace and outdoor living installations rather than irrigation. Repair kits and hand tools sold under the Champion name are meant to service the company's own valves and sprinkler heads already in the field.
Why Contractors Specify Champion
Contractors who maintain older irrigation systems often specify Champion parts. The company has kept many of its valve and sprinkler-head designs in production for decades, so a failed component can usually be matched and replaced without reworking the surrounding piping. Brass construction across much of the valve and fitting line holds up under the pressure swings and temperature changes typical of buried irrigation lines. That matters on commercial properties, where a callback means digging up landscaping a second time. Maintenance crews on golf courses and community landscapes can use the same repair-parts approach. They stock Champion valves and sprinkler internals so a crew can fix a zone without replacing the whole assembly. For contractors working on older Champion systems, long-standing parts compatibility reduces the guesswork in matching a replacement to what's already buried in the ground.
How to Choose Champion Products
Matching a replacement Champion valve or sprinkler head starts with the model number stamped or molded on the original part. Champion has produced multiple valve series over the decades that aren't interchangeable. Contractors replacing a bubbler or spray head should confirm the GPM rating and operating pressure range printed on the original component. Swapping in a different flow rate can throw off an existing zone's coverage. For new valve-box installations, brass anti-siphon or automatic anti-siphon valves suit exposed, above-grade locations, while inline and manual valves work for buried or in-line placements. Anyone specifying gas log lighter valves should check the local gas code and orifice size requirements before ordering. Champion's log lighter line is built for a different application than its irrigation valves and isn't interchangeable with them.
Frequently Asked Questions
Where is Champion Irrigation Products headquartered?
Champion was founded in Los Angeles, California, in 1937. It has since moved its headquarters to Memphis, Tennessee, while keeping its focus on irrigation valves, sprinklers, and related parts.
What types of valves does Champion make?
Champion's valve lineup includes anti-siphon valves, automatic anti-siphon valves, manual valves, inline valves, ball valves, hose bibs, sillcocks, and vacuum breakers for irrigation systems.
Are Champion sprinkler heads compatible with other brands?
Champion has kept many of its valve and sprinkler-head designs in production for decades, so parts can often be matched to older Champion components. A contractor matching an existing system should confirm the specific model number rather than assuming cross-brand compatibility.
Does Champion make anything besides irrigation parts?
Yes, Champion also produces gas log lighter valves and log lighter bars, a separate product line built for fireplace and outdoor living installations rather than irrigation.
Who typically installs Champion irrigation products?
Champion's customer base includes contractors, wholesalers, retailers, and homeowners, with the parts showing up on golf courses, agricultural fields, parking lots, and community landscaping projects.