Hayward Flow Control has manufactured industrial thermoplastic valves and process control products for close to 100 years. It was among the earliest producers of thermoplastic ball valves in the industry. Its engineering, manufacturing, customer support, and technical service operations run under one roof in the United States, with output reaching US, Canadian, and international markets. Hayward Flow Control holds ISO 9001:2015 accreditation through ANAB. Its equipment serves aquatics, mining, shipbuilding, and power generation. It also serves oil and gas, along with chemical processing and handling. Other markets include waste and water treatment. Surface finishing and metal plating facilities use it too. So do data center and semiconductor facilities.
Product Lines
SupplyHouse carries Hayward Flow Control's thermoplastic valve, fitting, and strainer lines. These include TBH Series true union ball valves, TC Series true union ball check valves, and BFA Series bulkhead fittings with EPDM gaskets. They also include YS Series Y-strainers and SB Series simplex basket strainers. The ball valve lineup spans PVC, CPVC, glass-filled polypropylene, and PVDF construction. Industrial models cover 1/4 inch through 6 inch (DN8 through DN150). Commercial models cover 1/2 inch through 4 inch (DN15 through DN100). A three-way true union ball valve line handles flow-diversion applications where a standard two-port valve won't work.
Why Contractors Specify Hayward Flow Control
Contractors working with corrosive or high-purity process water rely on Hayward Flow Control's thermoplastic construction because it resists the chemical attack and corrosion that degrade metal valves in the same service over time. The true union design on Hayward ball valves lets a technician remove the valve body from the line for service or replacement. The surrounding pipe run does not need to be cut, which reduces labor time on maintenance calls. A contractor can spec valves, fittings, and strainers in thermoplastic from Hayward Flow Control instead of mixing components from multiple manufacturers.
How to Choose Hayward Products
Material selection should follow the chemistry and temperature of the media running through the line. PVC handles general water and mild chemical service at lower temperatures. CPVC extends that range higher. PVDF and glass-filled polypropylene fit more aggressive chemical or higher-temperature applications. Line size and expected flow rate determine which valve series applies, since the industrial ball valve line covers a wider size range than the commercial line. For process lines fed by two or more sources, a three-way true union ball valve replaces a pair of standard valves and simplifies flow routing at the fitting. Strainer selection depends on the debris load expected in the line. A YS Series Y-strainer suits lighter-duty filtration ahead of a component like a pump or meter. An SB Series simplex basket strainer suits a heavier or more variable sediment load.
Frequently Asked Questions
What materials do Hayward Flow Control thermoplastic valves come in?
Hayward ball valves are available in PVC, CPVC, glass-filled polypropylene, and PVDF, so the material can be matched to the chemistry and temperature of the line.
What's the size range for Hayward industrial ball valves?
The industrial ball valve line covers 1/4 inch through 6 inch (DN8 through DN150), and the commercial ball valve line covers 1/2 inch through 4 inch (DN15 through DN100).
Why choose a true union ball valve over a standard ball valve?
A true union design lets the valve body come out of the line for service or replacement. The surrounding pipe does not need to be cut, which speeds up maintenance and reduces the pipe rework needed on a repair call.
When does a three-way ball valve make more sense than two standard valves?
A three-way true union ball valve handles flow diversion or mixing from a single fitting, replacing what would otherwise take two standard valves and extra pipe fittings.
Is Hayward Flow Control certified to a quality standard?
Yes, Hayward Flow Control holds ISO 9001:2015 accreditation through ANAB.