SpeedClean designs and manufactures maintenance tools built specifically for HVAC, plumbing, and general contracting professionals. Product development centers on practical field problems, from cleaning clogged evaporator and condenser coils to descaling hot water systems. The equipment is sized and built for daily use on a service truck.
Rather than general purpose cleaning equipment, the company concentrates on task specific tools that speed up routine maintenance calls. Its catalog is aimed at technicians who need portable, reliable equipment for coil cleaning, descaling, and mini split maintenance.
Product Lines
SpeedClean's core offering is the CoilJet line of coil cleaning systems, including the portable, rechargeable CJ-125 and a backpack mounted version for hands free operation on larger jobs. The Condenser Needle and CoilShot tools are built specifically for cleaning condenser coils in the field.
For scale removal, the BucketDescaler helps technicians clear limescale deposits from hot water systems and tankless water heaters. The Mini-Split Bib Kit is designed for cleaning mini split air handlers. The Dry Steam Coil and Surface Cleaner removes bacteria, dirt, and grease without chemicals. SpeedClean also supplies coil cleaning chemicals formulated to pair with its equipment.
Why Contractors Specify SpeedClean
Coil cleaning and descaling are recurring maintenance tasks, and tools built for that specific job tend to cut time on site compared to generic cleaning equipment. Portable, rechargeable designs let technicians carry a complete coil cleaning setup without hauling bulky equipment or running power cords.
A chemical free steam option gives contractors flexibility on jobs where chemical cleaners are restricted or where a customer prefers a non-chemical approach. Purpose built kits for mini split systems address a segment of the HVAC market that continues to grow. They give technicians a dedicated tool instead of adapting equipment meant for traditional split systems.
How to Choose SpeedClean Products
Start with the type of maintenance being performed. Coil cleaning calls for a CoilJet system or the Condenser Needle and CoilShot tools, while scale removal from hot water equipment calls for the BucketDescaler. Mini split maintenance is better served by the Mini-Split Bib Kit, which is sized for those air handlers.
Consider job volume and access when choosing between a handheld CJ-125 and the backpack coil cleaner, since the backpack version favors larger jobs where hands free operation matters. Where chemical use is a concern, the Dry Steam Coil and Surface Cleaner offers a chemical free alternative for coil and surface cleaning.
Frequently Asked Questions
What is the difference between the CoilJet CJ-125 and the backpack coil cleaner?
The CJ-125 is a portable, rechargeable handheld coil cleaning system, while the backpack model is worn on the back for hands free operation on larger cleaning jobs.
Can SpeedClean coil cleaning tools be used without chemicals?
Yes, the Dry Steam Coil and Surface Cleaner removes bacteria, dirt, and grease using steam without chemical cleaners.
What does the BucketDescaler do?
It removes limescale deposits from hot water systems and tankless water heaters.
What is the Mini-Split Bib Kit used for?
It is built for cleaning mini split air handlers, giving technicians a tool sized specifically for that equipment.
Does SpeedClean offer coil cleaning chemicals?
Yes. SpeedClean supplies coil cleaning chemicals formulated to pair with its equipment.