Apply to be a TradeMaster!
Main product image of Magnetic Capacitor Discharge Pen
Magnifying glass
Hover image to zoom

Magnetic Capacitor Discharge Pen

Brand:
Supco
SKU:
CAPDIS
Rating:
(19)
Q&A:
(0)
Magnetic Capacitor Discharge Pen
Magnifying glass
Hover image to zoom
$11.53 each
Out of Stock
Out of Stock
Get it Wed, Dec 9 - Wed, Dec 16
Free Shipping On orders over $99
Easy Returns No restocking fee for 90 days

Description

–
For discharging capacitors safely, without the risk of electrical shock.For professional use only.

Features:
  • LED indicator to let you know if capacitor is charged
  • Standard magnetic connector or alligator clip adapter
  • Intended for Professional Use ONLY

Specs

–
Product Type:

Tool

Light:

LED

Contact

+
Help Face

Questions?

Speak with a real person who will go out of the way to help!
Call or text 888-757-4774
Monday – Thursday
8am–7:45pm
Friday
9am–7:45pm
Saturday – Sunday
9am–5:45pm


You May Also Need

Magjumper Magnetic Test Leads (Blue)
SKU: MAG1BL
Supco

Product Reviews

4.58 out of 19 reviews
94% would recommend this product
4.58
out of 19 Reviews
94% would recommend this product
WRITE A REVIEW
5 star
84%
4 star
5%
3 star
0%
2 star
5%
1 star
5%
WRITE A REVIEW

Most Liked Positive Review

I recommend for all techs

For techs, I usually short the terminals to perform the discharge and recently did experience damaging a dual CAP by doing so. Decided to get one of these to prevent damage but more importantly to prevent sparking. The magnetic tip that inserts into the included alligator clip is a plus as it speeds up the service time. I recommend that depending solely on the LED may not be good practice. And do note that the discharge time is around 5 secs +/- 3; based on my use cases so far. Best to bridge the terminals with something like a insulated screw driver afterwards just as a precaution. Having said that , definitely highly recommended.
VS

Most Liked Negative Review

No reason for this to exist

If a motor is good, the cap will discharge through the motor windings making this device of no value. If the motor winding are open it is possible for the cap to hold a charge and for the cap to be damaged then discharged with a screwdriver. So what? If you are going to replace a motor you are always going to replace the cap anyway. Don't waste your money and tool bag space on this unnecessary tool.
Showing 1-10 of 19 reviews

Beware!

When you order parts that are not in stock they do not charge you at the time and hold your order until you confirm the credit card you already input. There email to confirm the CC only indicates there is an issue with your order, that is causing a delay. In there correspondence they say to call at your convenience.
Chewy
Dallas
1 months ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

It worked great.

The discharge pen worked great. Sadly, the capacitor wasn't the problem. On the bright side, I didn't get zapped by the old one because I was able to safely discharge it.
prh
Clayton, NJ
2 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Use this tool if put Safety First.

Sure beats discharging caps with a screwdriver.
Mick
Berlin, MD
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

must have tool in my bag

I use it to know cap is discharged for my safety
tec tom
dover .nj
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

For safety above all else

Pull up a slow motion, view of discharging a capacitor with a screwdriver and see all the small shrapnel that comes off the terminal ends that's why this tool exists
Steve
Mn
3 years ago
Was this review helpful to you?

Great buy- fast shipping

I've been using the screwdriver to discharge CAP, but decided to purchase this pen just to make sure the CAP got discharged properly. Great buy fast shipping
Roy
Oklahoma City
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Great tool

Don't listen to the 1 star review. He/She obviously has no idea and is going to get somebody hurt. Also probably never worked on York chillers with the huge capacitor bank that will kill you if you don't follow proper precautions and test!
BC
Richmond, VA
3 years ago
Was this review helpful to you?

As expected

Overpriced for what it is but I like having the correct tool. Wire and connector seem a bit delicate, though.
Gregory
NC
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

I would recommend to everyone that deals with capacitors

This is a great product it makes my job alot safer, and works as it states
Larry
Michigan
4 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

No reason for this to exist

If a motor is good, the cap will discharge through the motor windings making this device of no value. If the motor winding are open it is possible for the cap to hold a charge and for the cap to be damaged then discharged with a screwdriver. So what? If you are going to replace a motor you are always going to replace the cap anyway. Don't waste your money and tool bag space on this unnecessary tool.
Marty3006
Greenback, Tn
4 years ago
Was this review helpful to you?
Free Shipping
On orders over $99
We offer flexible shipping and scheduling options, up-to-date delivery estimates, and free ground shipping on any order over $99 to make sure your order gets to you on-time, for less.
Shipping Policy
Easy Returns
Returning items is as simple as 1-2-3
Ordered the wrong product? Item damaged in transit? Our 3-step process makes returning products easy – even up to a year after purchase – with no restocking fees on returns made within 90 days.
Return Policy