Chicago Fittings got its start in 1930, when the Kelly family began manufacturing specialty joining products for the natural gas and propane markets under Kelco Industries in Broadview, Illinois. Over the following decades the company moved through Woodstock and Belvidere before settling into its current Beloit, Wisconsin facility in 2015. In 2017, A.Y. McDonald Mfg. Co. acquired Chicago Fittings, folding nearly a century of gas-fitting experience into a larger manufacturing organization while keeping the Chicago Fittings name on its riser and transition-fitting product line.
Chicago Fittings focuses narrowly on the natural gas and propane distribution market, with a secondary presence in industrial hydraulics. Its Beloit plant is ISO 9001:2015 certified. The brand built its reputation on engineered transition and riser fittings that connect underground plastic gas piping to above-ground steel service lines. In this niche, joint integrity and corrosion resistance are critical for utility and contractor customers alike.
Product Lines
The core of the Chicago Fittings catalog is the X-Riser. The manufacturer markets it as the only natural gas and propane riser built with no underground joints, which reduces the number of potential leak points between the plastic main and the meter set. Around that flagship product, Chicago Fittings offers rigid risers, service heads, adapters, and a range of transition fittings that join polyethylene pipe to steel or copper service lines.
The product line is purpose-built for gas utility and propane distribution work. Most items are specified by exact size and pressure rating rather than browsed as a general catalog. Contractors and utility crews typically order Chicago Fittings components to match a specific riser height, pipe diameter, and connection type called out in a job's engineering drawings.
Why Contractors Specify Chicago Fittings
Gas utility contractors work under strict code requirements for underground joints. Every buried connection is a potential leak point that has to be located, excavated, and repaired if it fails. A riser built without underground joints simplifies both installation and long-term inspection. For this reason, crews doing new gas service installs or riser replacements often standardize on the X-Riser design.
ISO 9001:2015 certification at the Beloit manufacturing facility gives specifiers a documented quality-management system behind each fitting. This matters on utility-company approved-materials lists, where a manufacturer's certifications are part of the qualification package.
How to Choose Chicago Fittings Products
Start with the service type. Natural gas and propane installations have different pressure and material requirements, so confirm the fitting is rated for the specific gas being distributed before ordering. Next, match the riser or transition fitting to the exact pipe diameter and material on both sides of the connection. Chicago Fittings' transition pieces are sized to join specific combinations of polyethylene, steel, and copper.
Finally, check the required riser height against the meter set location and any local utility specifications. Gas utilities frequently maintain their own approved-materials lists that dictate which Chicago Fittings models can be used on their systems.
Frequently Asked Questions
What makes the Chicago Fittings X-Riser different from a standard gas riser?
The X-Riser is built as a semi-rigid assembly with no underground joints. The connection between the buried polyethylene main and the above-ground steel service line therefore has fewer potential leak points to inspect and maintain.
Is Chicago Fittings still an independent manufacturer?
No. A.Y. McDonald Mfg. Co. acquired Chicago Fittings in 2017, and the product line is now manufactured at an ISO 9001:2015 certified facility in Beloit, Wisconsin under the Chicago Fittings name.
Do Chicago Fittings products work for both natural gas and propane?
Yes, the company's risers and transition fittings are designed to serve both natural gas and propane distribution applications. The specific fitting and rating still need to match the gas type and pressure of the job.
What industries mainly use Chicago Fittings products?
Gas utility companies and propane distributors are the primary users, along with contractors performing new service installations, riser replacements, and meter set work on their behalf.
What types of products does Chicago Fittings offer?
Chicago Fittings offers the X-Riser, rigid risers, service heads, and adapters. It also offers a range of transition fittings that join polyethylene pipe to steel or copper service lines.