Niagara Conservation was founded in 1974 by William Cutler, who began developing water-saving plumbing devices from a home workshop years before federal low-flow standards existed. The company introduced its first product, a low-flow showerhead rated near 2.5 gallons per minute, in 1977.
Niagara Conservation is headquartered in Fort Worth, Texas, and has built its reputation around water conservation for plumbing fixtures used in residential and commercial construction. The manufacturer received the EPA WaterSense Manufacturer Partner of the Year award in 2011 and again in 2013 for its contributions to water efficiency initiatives.
Product Lines
SupplyHouse carries Niagara's toilet lineup, including Stealth and EcoLogic Technology models built around dual-flush operation, with average flush volumes as low as 0.65 gallons per flush and standard flush ratings of 1.28 gallons per flush. Niagara showerheads use Equiforce Technology and are offered in flow rates from 1.0 to 2.0 gallons per minute, in both fixed-mount and handheld configurations. Faucet aerators round out the lineup, giving plumbing contractors options for retrofitting fixtures to lower water consumption without swapping the entire fixture.
Why Contractors Specify Niagara
Plumbing contractors who work on water utility rebate programs or municipal retrofit projects often turn to Niagara. Its toilets and showerheads are engineered to meet WaterSense and low-flow code requirements. They still deliver consistent flush and spray performance. Niagara's Stealth toilets combine air and water in the flush cycle. Contractors can offer clients a fixture that meets aggressive water-reduction targets without the weak flush performance that caused callbacks on older low-flow models.
How to Choose Niagara Products
Selecting between Stealth and EcoLogic toilet models generally comes down to project requirements. Stealth models suit jobs where maximum water savings and dual-flush flexibility matter most. EcoLogic models fit budget-conscious specifications that still need to meet WaterSense criteria. For showerheads, matching the Equiforce flow rate, from 1.0 to 2.0 gallons per minute, to local plumbing code and the property type helps avoid change orders after installation. Aerator selection should follow the same logic, matching flow rate to fixture use and any water utility rebate program requirements tied to the job.
Frequently Asked Questions
What is the difference between Niagara's Stealth and EcoLogic toilet lines?
Stealth models combine air and water in the flush cycle and reach average flush volumes as low as 0.65 gallons per flush in dual-flush operation. EcoLogic Technology toilets fit budget-conscious specifications that still need to meet WaterSense criteria.
Are Niagara showerheads code-compliant for low-flow plumbing requirements?
Niagara showerheads with Equiforce Technology are engineered to meet WaterSense and low-flow code requirements. They are offered in flow rates from 1.0 to 2.0 gallons per minute, so installers can match the flow rate to local plumbing code and the property type.
Does Niagara make products beyond toilets and showerheads?
Yes. SupplyHouse carries Niagara faucet aerators. They give plumbing contractors a way to retrofit fixtures for lower water consumption without swapping the entire fixture.
Has Niagara received recognition for water conservation?
Niagara Conservation received the EPA WaterSense Manufacturer Partner of the Year award in 2011 and again in 2013. The awards recognized its contributions to water efficiency initiatives.
Where is Niagara Conservation based?
Niagara Conservation is headquartered in Fort Worth, Texas. The company was founded in 1974 to develop water-saving plumbing devices.