Apply to be a TradeMaster!
Main product image of Pick Up Stix Toilet Installation and Removal Tool
Magnifying glass
Hover image to zoom

Pick Up Stix Toilet Installation and Removal Tool

SKU:
PICKUPSTIX
Rating:
(64)
Q&A:
(0)
Pick Up Stix Toilet Installation and Removal Tool
Magnifying glass
Hover image to zoom
$55.00 each
In Stock
In Stock
Get 66 Mon, Oct 19
Order by 6PM, receive Monday
Free Shipping On orders over $99
Easy Returns No restocking fee for 90 days

Description

–

Product Note: This item has recently undergone a design change by the manufacturer, but functionality remains the same. Based on our current on-hand inventory, you may receive either the previous or updated design as we transition to the new version.


Advantages

  • Light weight & easy to store in tool kit
  • Fast and easy installation under bowls rim (Side to side or front to back)
  • Precision Lining up of T-Bolts
  • With PICK UP STIX® you now have a handle making the job of lifting and lowering of the water closet cleaner & easier with less slips

Who Will Benefit?

  • Ceramic Manufactures
  • Plumbers
  • Drain Technicians
  • Renovators
  • Flooring Installers
  • Home Handypersons


Increase Installer Confidence

Now with the use of PICK UP STIX® even the most difficult installation is done quickly, easily and with precision. Installation is a breeze. No more installer reluctance to promoting one-piece, heavier, or sleeker designed toilets which will increase manufactures high end sales.


Installer and Product Safety

  • Reduce back injuries
  • Reduce fixture breakage by minimizing slips
  • Increase handling ease
  • Minimize bacterial & bio-hazard contact

Specs

–
Product Type:

Installation Tool

Type:

Toilet Installation & Removal Tool

Help Face

Questions?

Speak with a real person who will go out of the way to help!
Call or text 888-757-4774
Monday – Thursday
8am–7:45pm
Friday
9am–7:45pm
Saturday – Sunday
9am–5:45pm


You May Also Need

Product Reviews

4.42 out of 64 reviews
87% would recommend this product
4.42
out of 64 Reviews
87% would recommend this product
WRITE A REVIEW
5 star
75%
4 star
13%
3 star
2%
2 star
2%
1 star
9%
WRITE A REVIEW

Most Liked Positive Review

I would by this product again

it does what it is supposed too, made it a lot easier to remove and install a new toilet...
VS

Most Liked Negative Review

Save your money

It's a nice idea but doesn't provide you with a better balanced grip on assembled toilets which is what most property managers and plumbers will encounter. Throw on some disposable gloves and grab where necessary and you'll be further ahead than buying this spring loaded stick. My recommendation would be to save up and buy a toilet cart or dolly.
Showing 1-10 of 64 reviews

This item is garbage!

Great idea poorly executed. Don't waste your money Even if you see guys recommending it on the socials
Jimbobob
Atlanta
2 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Great tool

Works great
Inzaghi
Ohio
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

No More Penguin Waddle

This tool is great. If you frequently remove toilets then you need this. Pair it with the Oatey Liquidlock and you won't even need a garbage bag.
Handyman
Pollock Pines, CA
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

The Supplier to Go To

We are very happy with the purchase. Highly recommend. Thank you !
WrenchHead
Los Angeles
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Nice

Helpful in avoiding the dreaded chip or broken toilet !
Mccr3328
Chicago
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Works great

I like it, great on nee installs! The black rubber is really stiff (think car tire). Makes lifting toilets so much more ergonomic. I will say tho, for removing existing toilets you may need to make sure the contact points are dry. I had a panic moment carrying a used toilet down the stairs and the handle shifted. 😅 It didn't come out but I haven't had that happen on new installs. So I think it was due to moisture. Would still recommend.
Tim the Plumber
Ct
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

Worked great - time and back saver

Worked perfectly for removing a toilet from a tight place that required 2 people but had no room for the 2nd person. I was able to lift and move the toilet effortlessly into an area where I could get help. It also helped getting the toilet out of the box!!!!
Bob
Grand Prairie
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

No definitely not it broke on me

It was not strong for a one peace toilet. 😔 drop it and broke tile too. And long gone but yea I got this and when using the tool the ends of the rubber came off and the spring was not strong enough and came off This tool could have worked. If the ends are a lot more stronger and part of the tool aluminum.
Sab
Puyallup wa
3 years ago
Was this review helpful to you?

I would buy this product again.

I use it to set and pull toilets and it works great.
Cwc plumbing co
So California
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?

A must have

I should have pulled the trigger on this years ago. Makes setting and removal safe and easy, definitely saves your back.
JBR
NC
3 years ago
Verified Buyer Icon
Verified Buyer
Was this review helpful to you?
Free Shipping
On orders over $99
We offer flexible shipping and scheduling options, up-to-date delivery estimates, and free ground shipping on any order over $99 to make sure your order gets to you on-time, for less.
Shipping Policy
Easy Returns
Returning items is as simple as 1-2-3
Ordered the wrong product? Item damaged in transit? Our 3-step process makes returning products easy – even up to a year after purchase – with no restocking fees on returns made within 90 days.
Return Policy