Plastic Oddities is a plumbing manufacturer headquartered in Forest City, North Carolina, where it produces plastic drainage components for professional installers. Rather than covering the full plumbing catalog, the company concentrates on parts that traditionally shipped in metal. These include floor drains, floor sinks, roof drains, cleanouts, closet flanges, and air gaps, each reengineered in molded plastic. The narrow, deep product focus gives plumbers a dedicated plastic alternative on jobs where corrosion resistance or weight matters more than a cast iron or bronze fitting would.
Product Lines
Plastic Oddities' catalog centers on drainage hardware built for both new construction and remodel work. Floor drains come in 3 inch, 4 inch, and 6 inch grate sizes. Floor sinks are available in round and square profiles to match different kitchen and utility room layouts. Closet flanges cover common toilet rough in configurations. They include the PAR 340 SS and the PFF106, PFF114, and PFF116 models. Both solvent weld and threaded connection options are carried through the cleanout line. Roof drains such as the PRD900 and SP61 round out the lineup for low slope commercial roofing applications. The company's PFSGA2 air gap fitting is a smaller but frequently specified item for dishwasher and reverse osmosis drain lines.
Why Contractors Specify Plastic Oddities
Plumbers reach for Plastic Oddities parts when a job calls for drainage hardware that won't corrode the way metal can in wet, high humidity environments. Molded plastic construction also cuts installation time since fittings are lighter to handle and easier to trim or adapt on site than rigid metal counterparts. Because the company's lineup is narrow and purpose built, contractors get application specific parts, like the round and square floor sink options. They avoid a one size fits all fitting that needs extra work to fit.
How to Choose Plastic Oddities Products
Selecting the right Plastic Oddities part starts with matching the fitting to the pipe size and connection type already in place. Cleanouts and closet flanges are offered in both solvent weld and threaded versions, so confirming which connection method the existing rough in uses before ordering avoids a mismatch. Floor drain and floor sink selection depends on the room. Floor drains come with 3 inch, 4 inch, or 6 inch grates, and floor sinks have a round or square footprint. Measuring the existing opening or checking the blueprint call out prevents an on site swap. For roof drain applications, the PRD900 and SP61 serve different roof configurations. Checking the building's roof slope and drain body size beforehand keeps installation on schedule.
Frequently Asked Questions
What connection types do Plastic Oddities cleanouts support?
Plastic Oddities cleanouts are offered in both solvent weld and threaded connection styles, letting plumbers match the fitting to the pipe joining method already used on the job.
What sizes are available for Plastic Oddities floor drains?
Plastic Oddities floor drains come with 3 inch, 4 inch, or 6 inch grates.
Does Plastic Oddities make floor sinks in more than one shape?
Plastic Oddities floor sinks are available in both round and square profiles. These match different kitchen and utility room layouts.
What closet flange models does Plastic Oddities offer?
Plastic Oddities' closet flange lineup includes the PAR 340 SS along with the PFF106, PFF114, and PFF116 models, covering common toilet rough in configurations.
What is the Plastic Oddities PFSGA2 fitting used for?
The Plastic Oddities PFSGA2 is an air gap fitting for dishwasher and reverse osmosis drain lines.