Sporlan is a manufacturer of refrigerant controls and components for air conditioning, heat pump, and commercial refrigeration systems. Founded in 1934 in St. Louis, MO as the Spoehrer-Lange Company, Sporlan introduced the Catch-All in 1947, the world's first molded core filter drier. Parker Hannifin acquired Sporlan Valve Co. in October 2004; Sporlan now operates as a division within Parker Hannifin's Climate and Industrial Controls segment, based in Washington, Missouri.
Product Lines
- Thermostatic Expansion Valves (TXV): For AC, heat pump, and refrigeration; replaceable thermostatic element; 12-mesh inlet strainer; external and internal equalizer options
- Electronic Expansion Valves: SER series (refrigeration); EDEV series (AC/heat pump, with integrated distributor and optional check valve)
- Solenoid Valves: Normally-open and normally-closed; stainless steel options; combined solenoid/check valve for heat pump liquid lines
- Catch-All Filter Driers: Industry's first molded core filter drier (1947); range of connection sizes and refrigerant capacities
- Sight glass and moisture indicator combinations
- Ball valves for refrigerant isolation
- Check valves, pressure regulating valves, refrigerant distributors
- Electronic superheat and subcooling controllers
Why Contractors Specify Sporlan
- 90-plus year track record in commercial refrigeration and AC controls
- Catch-All filter drier: industry standard since 1947, category that Sporlan originated
- Replaceable thermostatic element in TXVs: service the valve in the field without removing the body
- EDEV simplifies the refrigerant circuit by integrating EEV, distributor, and optional check valve
- Parker Hannifin global distribution and technical support network
How to Choose a Sporlan Component
For a TXV, match refrigerant type, system capacity, connection size, and equalizer configuration. For a filter drier, select the Catch-All size by system capacity and connection diameter. Replace the filter drier after a compressor burnout or open-system event. For a solenoid valve, use normally-closed for a liquid line, or a combined solenoid/check valve for heat pump reverse-cycle. For an electronic expansion valve, choose SER for refrigeration or EDEV for AC/heat pump variable-capacity systems.
Frequently Asked Questions
- When was Sporlan founded? Sporlan was founded in 1934 in St. Louis, MO, as the Spoehrer-Lange Company by Hermann Spoehrer and Harry Lange.
- Who owns Sporlan? Parker Hannifin acquired Sporlan in October 2004. Sporlan operates as a division within Parker Hannifin's Climate and Industrial Controls segment.
- What is the Catch-All? The Catch-All is a molded core filter drier introduced in 1947, the industry's first. It protects refrigerant systems from moisture and contaminants.
- What is a replaceable thermostatic element? It is the TXV sensing/actuating element. It can be replaced in the field without removing the valve body from the system piping.
- What is EDEV? EDEV stands for Electronic Distributor Expansion Valve. It combines an electronic expansion valve, an integrated distributor, and an optional check valve for AC and heat pump split systems.