Black Mamba makes disposable and reusable nitrile gloves built for industrial and trade work rather than general-purpose or medical use. The brand maintains regional sales coverage across the Southeast, Northeast, and Western United States, with a Southeast office at 1325 Calvary Creek Parkway SW in Gainesville, Georgia.
Black Mamba's core market is trade professionals who face chemical, abrasion, or tear hazards on the job. These include plumbing, HVAC, and other industrial applications where a standard disposable glove would not hold up.
Product Lines
SupplyHouse carries several lines of Black Mamba nitrile gloves. These include the standard Black Mamba Nitrile Gloves, Black Mamba Torque Grip Nitrile Gloves, and Black Mamba Raised Snake Skin Grip Nitrile Gloves. They are sold in sizes from small through 2XL in boxes of 100. The brand also makes Blue Mamba Nitrile Gloves, a lighter-colored version meant to make certain chemicals and solvents easier to spot on the glove surface.
Beyond gloves, Black Mamba's broader catalog includes disposable shoe covers, disposable clothing, and safety vests. This rounds out a line focused on disposable and semi-disposable personal protective equipment for trade work.
Why Contractors Specify Black Mamba
Contractors specify Black Mamba gloves when a job involves enough chemical exposure or abrasion that a standard latex or vinyl glove would tear or degrade too quickly. At 6.0 mils thick, the standard Black Mamba glove is built from a nitrile blend. The company markets it as offering three times the puncture resistance of latex or vinyl gloves of comparable thickness.
The Torque Grip and Raised Snake Skin Grip lines give contractors options built around wet or oily conditions where a smooth glove surface would slip. This matters for plumbing and HVAC techs handling pipe, fittings, or fasteners with hands that stay dry inside the glove but wet or greasy outside it.
How to Choose Black Mamba Products
Choosing between Black Mamba's glove lines mainly comes down to grip and visibility needs. The standard Black Mamba Nitrile Glove suits general chemical and abrasion resistance. The Torque Grip and Raised Snake Skin Grip versions add texture for handling wet, oily, or slippery materials. Techs who need to visually track chemical or solvent contact on a glove surface may prefer the lighter-colored Blue Mamba Nitrile Glove over the standard black version.
Sizing runs small through 2XL, sold by the box of 100. Crews should size gloves the same way they would any other PPE. Base the choice on hand size and dexterity needs for the specific task rather than defaulting to a single size for the whole crew.
Frequently Asked Questions
How thick are Black Mamba nitrile gloves?
The standard Black Mamba Nitrile Glove is 6.0 mils thick, which the company markets as giving three times the puncture resistance of comparable-thickness latex or vinyl gloves.
What is the difference between Black Mamba and Blue Mamba gloves?
Blue Mamba Nitrile Gloves use a lighter color than the standard Black Mamba glove. This makes it easier to spot certain chemicals and solvents that contact the glove surface during a job.
What sizes do Black Mamba gloves come in?
Black Mamba gloves are sold in sizes from small through 2XL, packaged in boxes of 100.
Are Black Mamba gloves meant for wet or oily work?
The Torque Grip and Raised Snake Skin Grip lines add textured surfaces specifically for handling wet, oily, or slippery materials, which the smooth standard glove is not built for.
Does Black Mamba make anything besides gloves?
Yes. Black Mamba's broader product line includes disposable shoe covers, disposable clothing, and safety vests in addition to its nitrile glove lines.