Flamco is a hydronic systems manufacturer that got its start in 1956 producing wall brackets and pipe hangers. The company has since grown into a supplier of expansion tanks, air and dirt separation equipment, and water treatment products. These products serve heating and cooling systems. Flamco became part of Aalberts Hydronic Flow Control in 2014, joining the broader Aalberts N.V. group.
Flamco's products serve residential, commercial, and industrial building systems, with a focus on components that keep hydronic heating and cooling loops running smoothly under pressure.
Product Lines
Flamco's product line centers on expansion tanks for pressurized hydronic systems, including its commercial range and the BaseFlex series. The brand also makes air and dirt separators, such as the Smart Series and XStream Series. These remove trapped air and particulate from closed loop piping.
Additional product categories include air vents, hydraulic separators, vacuum deaerators, near boiler trim kits, and stainless steel components for boiler and hydronic installations. Flamco rounds out its lineup with water treatment products, including inhibitors, system cleaners, and water testing kits, plus accessories like fill valves and backflow preventers.
Why Contractors Specify Flamco
Contractors working on closed loop hydronic systems specify Flamco for its expansion tanks and air/dirt separators. They are built specifically for the pressure and flow conditions found in heating and cooling loops, rather than adapted from a general purpose plumbing product.
Pairing an expansion tank with a matched separator from the same manufacturer also simplifies sizing and installation, since the components are designed to work together within one system design. For boiler retrofit work, Flamco's near boiler trim kits and stainless steel components give contractors a single source for the smaller parts a hydronic connection needs.
How to Choose Flamco Products
Selecting an expansion tank starts with system volume and operating pressure. Flamco's commercial range covers larger systems, while the BaseFlex series is sized for smaller residential and light commercial installations.
For air and dirt removal, the Smart Series suits standard closed loop systems, while the XStream Series is built for the higher flow rates found in larger commercial systems. Contractors should also check whether a project needs vacuum deaeration for continuous air removal or a standard air vent for point of use venting. The two serve different roles in a hydronic system.
Frequently Asked Questions
What was Flamco's first product?
Flamco began in 1956 by producing wall brackets and pipe hangers before expanding into hydronic system components.
Is Flamco part of a larger company?
Yes. Flamco became part of Aalberts Hydronic Flow Control in 2014, which operates under the Netherlands based Aalberts N.V. group.
What's the difference between Flamco's Smart Series and XStream Series separators?
The Smart Series is built for standard closed loop hydronic systems, while the XStream Series is designed for the higher flow rates found in larger commercial installations.
Does Flamco make water treatment products?
Yes. Flamco's water treatment line includes system inhibitors, cleaners, and water testing kits for hydronic loops.
What is the BaseFlex series used for?
BaseFlex is Flamco's expansion tank series sized for smaller residential and light commercial hydronic systems.