Kamco is a manufacturer of professional power flushing machines, power flushing chemicals, and descaling equipment for hydronic heating systems, radiant floor circuits, and heat exchanger cleaning. Kamco is the UK's leading supplier of professional power flushing equipment. The Clearflow product line includes compact portable machines and high-capacity commercial models, supported by system cleaners, inhibitors, scale removers, and neutralizers. For heating contractors performing hydronic system cleaning, descaling, or commissioning, Kamco provides the flow, pressure, and chemical compatibility needed to restore system performance.
Product Lines
Clearflow CF20 Compact Power Flushing Machine
The Kamco Clearflow CF20 Compact is a portable handheld power flushing machine for residential and light commercial applications. It cleans hydronic heating systems, flushes underfloor radiant circuits, and descales heat exchangers. The compact form factor allows access to tight mechanical rooms. The CF20 circulates water and flushing chemicals through the heating system. This purges sludge, scale, and corrosion deposits from the pipework and components.
Clearflow CF40, CF90, and CF210 Power Flushing Machines
Kamco Clearflow CF40, CF90, and CF210 are professional-grade machines for higher-capacity hydronic system cleaning. The CF40 covers standard residential and small commercial applications. The CF90 and CF210 address larger commercial heating systems with higher flow rates and more aggressive flushing capability.
Kamco Power Flushing Chemicals
Kamco power flushing chemicals include four types. System cleaners remove sludge and organic deposits. Descalers treat mineral scale in boilers and heat exchangers. Inhibitors provide post-flush corrosion protection. Neutralizers allow safe disposal after descaling. They are formulated for compatibility with copper, steel, aluminum, and brass components in residential and commercial hydronic heating systems.
Why Contractors Specify Kamco
Heating contractors specify Kamco because the Clearflow machine range covers power flushing from compact residential work to commercial system cleaning, supported by a complete chemical line. The CF20 Compact's portable form factor suits residential boiler rooms and tight-access applications. The Clearflow process is a documented methodology for purging sludge, scale, and corrosion deposits, restoring heat distribution efficiency and extending system life. Kamco is the UK market leader in professional power flushing equipment.
How to Choose a Kamco Power Flushing Machine
The most important decision variable is the system size. The CF20 Compact is right for residential boiler systems, small radiant circuits, and tight-access applications. The CF40 is for larger residential systems or light commercial hydronic systems where higher flow capacity reduces job time. The CF90 and CF210 address commercial heating systems with large loop volumes. For chemical selection: new system commissioning requires a cleaner plus inhibitor. Older systems with scale need a descaler, then neutralizer, then inhibitor.
Frequently Asked Questions
Where is Kamco equipment manufactured?
Kamco is a UK manufacturer of professional power flushing equipment. It is recognized as the UK's leading supplier in this category.
What types of chemicals does Kamco offer?
Kamco offers system cleaners, descalers, inhibitors, and neutralizers. System cleaners remove sludge and organic deposits. Descalers treat mineral scale in boilers and heat exchangers. Inhibitors provide post-flush corrosion protection. Neutralizers allow safe disposal after descaling.
What is the difference between the Clearflow CF20 Compact and CF40?
The CF20 Compact is a portable handheld machine for residential boiler systems and tight-access applications where compact size matters. The CF40 is a larger-capacity machine for residential systems where a higher flow rate reduces job time, and for light commercial systems that exceed the CF20's practical capacity. Both use the Kamco Clearflow power flushing methodology.
What heating systems can Kamco Clearflow machines be used on?
Kamco Clearflow machines can be used on closed-loop hot water heating systems. These include residential boiler systems with radiators or fan coil units, underfloor radiant circuits, and commercial hydronic loops. They can also descale heat exchangers. Verify that system materials are compatible with the Kamco chemical before beginning the flushing protocol.
What Kamco chemicals are needed for a residential power flushing job?
A standard residential job requires a Kamco system cleaner to remove sludge during the flush, followed by a Kamco inhibitor for post-flush corrosion protection. If scale is present, add a Kamco descaler and then a neutralizer before the inhibitor.
What does the Kamco Clearflow process do?
The Clearflow process is a documented methodology for purging sludge, scale, and corrosion deposits from hydronic heating systems. It restores heat distribution efficiency and extends system life.