Davey was established in 1934 as a one-man automotive electrical workshop in Carlton, Victoria, Australia. It has grown into a water pump and pressure system manufacturer that now exports to more than 50 countries. The company is part of Waterco Limited.
Davey serves residential, agricultural, commercial, and industrial customers. Its applications include water pressure, fire protection, pool and spa, and irrigation.
Product Lines
Davey's product range carried on SupplyHouse includes domestic water pumps and pressure systems, pool and spa equipment, and irrigation systems. It also includes commercial pumping solutions and the Firefighter line of fire safety pumps. The range also includes water treatment and controllers, plus rainwater harvesting controllers.
Why Contractors Specify Davey
Contractors specify Davey pumps because the manufacturer holds both ISO 9001 quality certification and ISO 14001 environmental management certification. It also builds to Lean manufacturing principles. This gives a documented quality process behind residential and commercial pump installations.
The product range spans domestic pressure systems through commercial and fire protection pumps. A contractor working across residential and light commercial jobs can often stay with one manufacturer's pump line rather than switching brands by application.
How to Choose Davey Products
Selecting a Davey pump starts with the application category: domestic water pressure, pool and spa, fire protection, irrigation, or commercial pumping. Match that category to the corresponding product line. Do not assume one pump model covers multiple use cases.
Fire protection installations should be matched to the Firefighter line specifically, since fire pumps carry different performance and listing requirements than a standard domestic pressure pump. Rainwater harvesting and water treatment jobs are supported by Davey's dedicated controller line rather than a general purpose pump controller.
Frequently Asked Questions
What is the Firefighter line used for?
The Firefighter line is Davey's range of fire safety pumps built for fire protection system applications rather than general domestic water use.
Does Davey make pumps for both residential and commercial use?
Yes. Davey manufactures pumps for residential, agricultural, commercial, and industrial customers. Its applications include water pressure, fire protection, pool and spa, and irrigation.
Where was Davey established?
Davey was established in 1934 in Carlton, Victoria, Australia. It is now part of Waterco Limited.
Does Davey make products for pool and spa applications?
Davey's product range includes pool and spa equipment alongside its water pressure, fire protection, and irrigation lines.
What quality certifications does Davey hold?
Davey holds ISO 9001 quality certification and ISO 14001 environmental management certification.