Eccotemp is a manufacturer of tankless water heaters, including portable outdoor units, whole-home indoor gas units, and electric tankless models for residential and light commercial applications. Founded in 2004 and headquartered in Summerville, South Carolina, Eccotemp is a family-owned company recognized as the number-one seller of portable tankless water heaters in North America. Eccotemp products are sold at more than 5,000 retailers across North America, Europe, and Australia. All Eccotemp gas tankless water heaters are CSA certified for the United States and Canada.
Product Lines
Eccotemp L5 Portable Tankless Water Heater
The Eccotemp L5 is a portable outdoor-use propane tankless water heater for camping, outdoor showers, livestock washing, and remote job site applications. It connects to a portable propane cylinder, uses D-cell batteries for ignition, and requires a garden hose water supply. It is for outdoor use only. The L5 is Eccotemp's entry point for portable hot water and one of the most widely distributed portable tankless heaters in North America.
Eccotemp SmartHome SH22 Propane Tankless Water Heater
The Eccotemp SmartHome SH22 is a propane indoor whole-home tankless water heater rated at 6.8 GPM. Wi-Fi connectivity allows remote temperature control via mobile app. It is designed for residential whole-home hot water delivery with connected control.
Eccotemp Builder Series Outdoor Propane Tankless Water Heater
The Eccotemp Builder Series Outdoor is a propane tankless water heater rated at 6.8 GPM for outdoor installation in residential whole-home applications. It is positioned for new construction and light renovation in climates where outdoor unit mounting is appropriate.
Eccotemp 20HI Indoor Natural Gas Tankless Water Heater
The Eccotemp 20HI is a natural gas indoor tankless water heater rated at 6.0 GPM for residential whole-home applications. CSA certified for use in the United States and Canada.
Why Contractors Specify Eccotemp
Plumbing contractors specify Eccotemp because the brand is CSA certified for the US and Canada. It also covers both propane and natural gas configurations for residential whole-home hot water. Eccotemp is the number-one seller of portable tankless water heaters in North America, sold at more than 5,000 retailers. The SmartHome series adds Wi-Fi connected control for residential customers. Eccotemp is a US-based family-owned company founded in 2004 and headquartered in Summerville, South Carolina.
How to Choose an Eccotemp Tankless Water Heater
The most important decision variables are installation location (indoor vs. outdoor), fuel type (propane vs. natural gas), and required flow rate in GPM. For portable applications without a permanent gas line, the L5 Portable connects to a portable propane cylinder with no venting or permanent installation. For indoor whole-home propane, the SH22 (6.8 GPM) adds Wi-Fi control. For outdoor whole-home propane, the Builder Series Outdoor (6.8 GPM) is designed for exterior mounting. For indoor whole-home natural gas, the 20HI (6.0 GPM) is the natural gas option. Flow rate matching is critical: verify peak GPM demand against rated output at local incoming cold water temperature.
Frequently Asked Questions
Where is Eccotemp headquartered and when was it founded?
Eccotemp was founded in 2004 and is headquartered in Summerville, South Carolina. It is family-owned and the number-one seller of portable tankless water heaters in North America. Its products are sold at more than 5,000 retailers across North America, Europe, and Australia.
Are Eccotemp tankless water heaters CSA certified?
All Eccotemp gas tankless water heaters are CSA certified for use in the United States and Canada. Verify the specific model's CSA certification scope on the product label before installation.
What is the flow rate of the Eccotemp SH22 SmartHome?
The SH22 is rated at 6.8 GPM on propane. Actual delivered flow at a given temperature rise depends on local incoming cold water temperature.
Can Eccotemp tankless water heaters be installed indoors?
Some models are indoor and some are outdoor-only. The L5 Portable is outdoor-use only. The SH22 and 20HI are indoor installation models with appropriate venting requirements. Verify each model's indoor/outdoor classification before siting the unit.
What fuel types does Eccotemp offer for whole-home tankless water heaters?
Eccotemp offers propane (SH22, Builder Series Outdoor) and natural gas (20HI) for whole-home residential tankless. Verify fuel type matches the available supply before ordering.
What does the Eccotemp L5 Portable need to operate?
The L5 connects to a portable propane cylinder and uses D-cell batteries for ignition. It requires a garden hose water supply. The L5 is for outdoor use only.