Falcon Stainless built its reputation manufacturing flexible stainless steel water and gas connectors for the plumbing and HVAC trades. The brand now operates under RectorSeal, a subsidiary of CSW Industrials. RectorSeal positions Falcon Stainless within its broader Whole Home Connector Solutions lineup, which spans water connectors, gas connectors, and thermal expansion tanks.
The stainless steel construction across the line is built to stand up to the demands of both residential and commercial installations. Falcon Stainless connectors show up on boilers, water softeners, water heaters, and other pieces of equipment where a flexible, corrosion-resistant connection matters.
Product Lines
Falcon Stainless water connectors are flexible, stainless steel lines designed for commercial and residential applications. These include boilers, water softeners, tanked and tankless water heaters, pumps, and water treatment systems. Gas connectors use a coated stainless steel construction. They cover an even broader range of appliances, including gas ranges, dryers, water heaters, furnaces, tankless water heaters, boilers, fireplaces, fire logs, and space heaters.
The Big Red line of commercial kitchen gas connectors adds a PVC coating for protection against abrasion, cuts, and impact, and carries an NSF listing for foodservice environments. Falcon Stainless also makes thermal expansion tanks, which address the closed-loop conditions created when a backflow preventer or check valve is installed on a water heater or boiler system.
Why Contractors Specify Falcon Stainless
Contractors specify Falcon Stainless connectors because the corrugated stainless steel construction holds up in tight mechanical rooms and crawlspaces. Connectors there may get bumped, flexed, or exposed to moisture over years of service. The gas connector lineup's coverage, from residential ranges to commercial boilers, means one supplier can handle most of the gas-appliance connections on a job instead of mixing brands.
In commercial kitchens, the Big Red line's NSF listing and abrasion-resistant coating matter because foodservice equipment gets moved, cleaned, and inspected more often than a typical residential setup. Pairing a thermal expansion tank with a water heater or boiler installation also helps address the pressure buildup from a closed-loop system. That detail is easy to miss without checking for a backflow preventer or check valve already on the line.
How to Choose Falcon Stainless Products
Confirming whether the application calls for a water connector or gas connector comes first. Water connectors are sized for boilers, water heaters, softeners, pumps, and treatment equipment. Gas connectors are rated separately for appliances like furnaces, dryers, and fireplaces. Length and diameter matter for a clean installation. Measuring the actual run between the shutoff and the appliance before ordering avoids a connector that's stretched too tight or coiled with excess slack.
For commercial kitchen gas connections, the Big Red PVC-coated line is worth specifying over a standard connector given the added abrasion resistance and NSF listing. Any water heater or boiler installation with a backflow preventer or check valve already in place should get a thermal expansion tank sized to the system. Otherwise, that closed-loop condition can push pressure past safe limits.
Frequently Asked Questions
What's the difference between Falcon Stainless water connectors and gas connectors?
Water connectors use flexible stainless steel construction and are sized for equipment like boilers, water heaters, softeners, and pumps. Gas connectors use a coated stainless steel construction and are rated for gas appliances such as furnaces, ranges, dryers, and fireplaces.
What is the Big Red line used for?
Big Red is Falcon Stainless's line of PVC-coated gas connectors built for commercial kitchens. The coating adds resistance to abrasion, cuts, and impact, and the line carries an NSF listing for foodservice environments.
When does a water heater or boiler need a thermal expansion tank?
A thermal expansion tank is needed when a backflow preventer or check valve creates a closed-loop system on the water heater or boiler. Without one, the pressure created by heated water expansion has nowhere to go.
Is Falcon Stainless still an independent company?
No. Falcon Stainless now operates under RectorSeal, a plumbing, HVAC, and electrical products manufacturer that's a subsidiary of CSW Industrials.
What equipment can use a Falcon Stainless gas connector?
The gas connector line covers gas ranges, dryers, water heaters, furnaces, tankless water heaters, boilers, fireplaces, fire logs, and space heaters.