Firomatic is a line of fusible fire safety valves manufactured by R.W. Beckett Corporation, built to automatically shut off oil flow from a tank when a fire raises the temperature past a set threshold. Beckett operates in the United States with Canadian operations. Firomatic valves are required by NFPA 31 on residential oil heating installations in the United States and by CSA B139-15 in Canada.
The fusible link at the heart of each valve melts at a fixed temperature. Depending on the model, this is typically 165 degrees Fahrenheit or 200 degrees Fahrenheit. The valve then closes and cuts off fuel to the fire.
Product Lines
Firomatic Fusible Inline Valves are brass. They are available in flare and threaded connections from one quarter inch to one inch, with UL listed models rated at 165 degrees Fahrenheit or 200 degrees Fahrenheit. Firomatic Fusible Burner, or Angle, Valves add a second layer of protection at the burner. They are available with three eighths inch and one half inch flare fittings and a one quarter inch NPT outlet across three length options.
Firomatic Fusible Tank Valves are bronze castings sized for a one half inch NPT tank bottom outlet and ship with the male nipples needed for installation. Certain UL 842 listed models across the line are certified for biodiesel blends up to B20.
Why Contractors Specify Firomatic
Oil heat technicians specify Firomatic valves because NFPA 31 requires a fusible valve on most residential oil tank installations. Firomatic also carries the cULus and UL 842 listings inspectors look for on a job. Because the valve line spans tank, inline, and burner locations, a technician can add fire protection at more than one point in the same fuel line without switching manufacturers.
Biodiesel compatible models matter increasingly as more oil heat customers move to B20 blends. Having that compatibility documented in the UL 842 listing keeps an installation compliant as fuel blends change.
How to Choose Firomatic Products
Choosing among Firomatic valves starts with the location in the fuel line. A tank bottom outlet calls for a Fusible Tank Valve sized to the one half inch NPT connection. A supply line calls for a Fusible Inline Valve sized between one quarter inch and one inch. The burner itself calls for a Fusible Burner, or Angle, Valve.
Temperature rating and connection size should match the existing installation and the governing code, whether NFPA 31 in the United States or CSA B139-15 in Canada. A biodiesel installation should confirm the UL 842 B20 listing before selecting a model.
Frequently Asked Questions
What does a Firomatic fusible valve do?
A Firomatic fusible valve automatically shuts off oil flow from a tank when the fusible link melts at a set temperature during a fire. This cuts fuel to the source before it can feed further damage.
Are Firomatic valves required by code?
Yes. NFPA 31 requires a fusible valve on most residential oil heating installations in the United States, and CSA B139-15 carries the same requirement in Canada.
What is the difference between an inline valve and a tank valve?
A Fusible Inline Valve installs in the supply line and comes in sizes from one quarter inch to one inch. A Fusible Tank Valve is a bronze casting built for the one half inch NPT outlet at the tank bottom.
Do Firomatic valves work with biodiesel blends?
Certain UL 842 listed Firomatic models are certified for biodiesel blends up to B20, so checking the listing on a specific model confirms biodiesel compatibility before installation.
What temperature ratings are available on Firomatic valves?
Firomatic fusible links are commonly rated to close at 165 degrees Fahrenheit or 200 degrees Fahrenheit, depending on the model selected.