IPS Corporation was founded in 1954 and is headquartered in Compton, California. The company built its early reputation on solvent cement chemistry, patenting what it describes as the first solvent cement formulated to join PVC pipe in 1958.
Since then, IPS has grown into a manufacturer with roughly 700 employees selling more than 10,000 products in over 90 countries. Centerbridge Partners acquired the company in 2021, and IPS has continued expanding manufacturing capacity since, including a solvent cement plant added in the Netherlands in 2025.
Product Lines
IPS is best known for Weld-On solvent cements, primers, and cleaners used to join PVC, CPVC, and ABS piping systems, a category the company has manufactured since its founding. Beyond solvent cements, the IPS portfolio covers rough plumbing and repair products. It also includes water damage prevention systems and drainage and ventilation components.
SupplyHouse also carries several brands under the IPS umbrella: Water-Tite, Studor, Guy Gray, AB&A, Roof Top Blox, and FloodStop. These span categories from plumbing carriers and vents to leak detection and roofing accessories. The SCIGRIP division adds structural adhesives to the broader IPS catalog for industrial applications.
Why Contractors Specify IPS Corporation
Plumbing contractors often standardize on Weld-On solvent cement for its decades of documented field history joining PVC and CPVC pipe. That history goes back to the original 1958 patent. Such a track record carries weight on inspected jobs where the cement joint is a critical part of the system.
Since 2009, IPS has also moved its solvent cement and primer lines toward lower-VOC formulations. This matters in jurisdictions with tighter indoor air quality or emissions rules on job sites. Sourcing the core Weld-On line and adjacent brands such as Studor and FloodStop from one manufacturer also simplifies purchasing. This helps a plumbing contractor working across drainage, venting, and leak protection on the same job.
How to Choose IPS Corporation Products
Solvent cement selection depends on pipe material and application. PVC, CPVC, and ABS each require a cement formulated for that plastic. Using the wrong cement can produce a joint that looks solid but fails under pressure. Primer compatibility and cure time also vary by cement type and pipe diameter.
For related IPS product lines, matching the component to the piping system matters just as much. A Studor air admittance valve has to match the vent stack diameter it is replacing. A FloodStop shutoff system needs to match the water line size and the sensor placement the job requires. Confirming pipe size and application before ordering avoids a mismatched part on install day.
Frequently Asked Questions
When was IPS Corporation founded?
IPS Corporation was founded in 1954 and is headquartered in Compton, California.
What is Weld-On?
Weld-On is the IPS brand name for its solvent cements, primers, and cleaners used to join PVC, CPVC, and ABS plastic piping.
Who owns IPS Corporation?
Centerbridge Partners acquired IPS Corporation in 2021.
What other brands does IPS Corporation manufacture?
IPS manufactures Water-Tite, Studor, Guy Gray, AB&A, Roof Top Blox, and FloodStop, along with the SCIGRIP structural adhesives division.
Does IPS Corporation make low-VOC products?
Yes. The company has been shifting its solvent cement and primer lines toward lower-VOC formulations since 2009.