Everpure has been in the water filtration business since 1933 and now operates as a brand under Pentair, a company focused on residential, commercial, and industrial water solutions. Everpure is best known among foodservice operators and facilities managers, though its filtration line also extends into residential water treatment.
The brand's long run in commercial filtration has made it a familiar name to consultants, dealers, and equipment manufacturers. They specify water treatment for restaurants and other foodservice operations. In these settings, filtered water quality affects everything from ice and coffee to fountain beverages.
Product Lines
Everpure's commercial lineup covers four main categories. These are complete filtration systems, replacement filter cartridges, filtration heads and minifolds for building out modular, scalable setups, and water softeners for high-capacity scale reduction. The cartridges use a commercial-grade aluminum casing built for repeated servicing in busy kitchens.
On the application side, Everpure filters are built for ice machines, coffee and espresso equipment, drinking water stations, fountain beverage lines, and steam equipment. Each is tuned to reduce suspended particles, chlorine, chloramines, and other odor-causing compounds specific to that use.
Why Contractors Specify Everpure
Contractors and facilities managers specify Everpure for its filtration heads and minifolds. These let a system scale from a single fountain line to a full kitchen setup without redesigning the plumbing each time. That modularity matters in foodservice retrofits where equipment gets added or swapped over time.
Nearly a century in the commercial filtration space has also built a service network and a replacement cartridge supply chain. This keeps maintenance predictable. Foodservice operators rely on that because a filtration failure can shut down ice or beverage service.
How to Choose Everpure Products
Match the filtration system to the application first. Ice machines, coffee and espresso lines, drinking water, fountain beverages, and steam equipment each call for a different cartridge configuration built around that water use. For a multi-fixture kitchen, a filtration head or minifold setup is worth considering over separate single-point systems, since it centralizes servicing.
Water softeners are the right call when scale buildup, not just taste or particulates, is the primary concern. This is particularly true for equipment like steamers and combi ovens that are sensitive to hard water. Replacement cartridges should be sourced as genuine Everpure parts to keep filtration performance consistent with what the original system was rated for.
Frequently Asked Questions
How long has Everpure been making water filtration systems?
Everpure has been in the water filtration business since 1933 and now operates as a Pentair brand.
Is Everpure only for restaurants?
Everpure is best known in foodservice and commercial kitchens, but its filtration line also extends into residential water treatment.
What is a filtration minifold used for?
It's a modular component that lets a kitchen scale its Everpure filtration setup from a single line to multiple fixtures without redesigning the plumbing.
Does Everpure make water softeners?
Yes. Everpure's lineup includes high-capacity water softeners built to reduce scale buildup on equipment like steamers and combi ovens.
What applications does Everpure filtration cover?
Everpure builds filtration for ice machines, coffee and espresso equipment, drinking water, fountain beverages, and steam equipment.