Revcor has built fan blades and airflow components since 1946. That is more than 75 years in a niche corner of HVAC manufacturing. Most contractors do not think about it until a unit needs a replacement blade. The company is headquartered in Carpentersville, Illinois, where it designs, builds, and continues acquiring the specialized tooling that airflow component manufacturing requires.
Revcor has developed more than 100,000 airflow solutions over its history, working directly with OEM engineering teams rather than selling only through the aftermarket. Custom configuration work makes up a large share of that history. The company reports more than one million distinct product configurations built to customer specification. That reflects how specific fan blade and blower requirements can get across different equipment platforms.
Product Lines
Revcor's catalog centers on fan blades in small, condenser, and large configurations. They are sized for residential and commercial air conditioning and heating equipment that needs blade replacements in the field. Blower wheels round out the lineup in light duty, medium duty, heavy duty, and crossflow versions. Complete blower assemblies, including housings and inlet rings, are available for jobs that need more than a standalone wheel. Riveted condenser fan blades in particular see wide use across residential and commercial air conditioning units, heat pumps, and rooftop equipment.
Why Contractors Specify Revcor
Revcor's quality figures give contractors an unusual data point for a component this specialized. The company reports 48 defective parts per million and a 98 percent on-time shipment rate. For a fan blade or blower wheel, the wrong size or an out-of-balance component means a return trip. Those numbers matter more than they might for less critical components. Revcor also serves industries beyond HVAC, including agriculture, food service, and transportation. Its engineering has therefore been tested across a wider range of operating conditions than a single-industry supplier would see.
How to Choose Revcor Products
Matching a Revcor fan blade or blower wheel to a job starts with confirming the exact equipment platform. The company builds distinct blade families for small, condenser, and large-diameter applications rather than a single universal design. Blower wheel selection depends on duty cycle. Light duty, medium duty, and heavy duty versions are rated for different runtime and load conditions. Crossflow wheels are reserved for equipment specifically designed around that airflow pattern. When a standalone wheel will not fit the existing housing, use a complete blower assembly with the housing and inlet ring. This avoids compatibility problems from mixing components from different manufacturers.
Frequently Asked Questions
How long has Revcor been in business?
Revcor was founded in 1946 and has been designing and manufacturing airflow components for more than 75 years.
Where is Revcor located?
Revcor is headquartered in Carpentersville, Illinois.
Does Revcor sell only fan blades?
No, the company also manufactures blower wheels in multiple duty ratings and complete blower assemblies, including housings and inlet rings.
What industries use Revcor components?
Beyond HVAC and air conditioning, Revcor components are used in agriculture, appliance manufacturing, food service, refrigeration, and transportation equipment.
How does Revcor support custom applications?
The company works directly with OEM engineering teams and reports having developed more than 100,000 airflow solutions across its history, in addition to running its own airflow testing labs.