Thermo Manufacturing was incorporated in 1992 by Darryl L. Snyder, an HVAC contractor and sheet metal journeyman who built the company around his own installation experience. Its first product, ThermoPan, was designed as a lighter, sound absorbing alternative to sheet metal for return air ducts built between floor joists and stud cavities. The company has since grown its catalog while staying focused on materials that speed up duct installation.
Product Lines
SupplyHouse carries Thermopan's core return air duct material along with the headers, saddles, and connectors used to tie ductwork sections together. The line also includes hanging straps, brackets, and snap clamps for securing panning in place, plus tapes, sealants, and insulation materials for sealing seams. Thermopan rounds out its catalog with grilles, registers, diffusers, levelers, and frames for finishing a return air system.
Why Contractors Specify Thermopan
Installers use Thermopan panning instead of sheet metal because it is lighter to carry and cut on site. This speeds up return air duct construction between joists and stud cavities. The corrugated, aluminum faced material also absorbs sound, which cuts down on the rattle and vibration noise that sheet metal ductwork can carry through a building. Because the panels come pre-cut, crews spend less time fabricating custom sections in the field.
How to Choose Thermopan Products
Measure the joist or stud cavity width and depth before ordering, since Thermopan panning comes in set widths and sizes meant to fit standard framing dimensions. Use the matching headers, saddles, and connectors from the same line so seams seal properly instead of mixing components from different systems. For exposed sections, add the tapes and sealants made for the panning material rather than a general purpose duct tape. The seal needs to hold against the vibration and temperature swings of a return air run.
Frequently Asked Questions
Who founded Thermopan?
Thermopan is a product line from Thermo Manufacturing, a company incorporated in 1992 by Darryl L. Snyder, an HVAC contractor and sheet metal journeyman.
What is Thermopan used for?
Thermopan is a lightweight, sound absorbing material used in place of sheet metal to build return air ducts between floor joists and stud cavities.
Does Thermopan come pre-cut?
Yes, Thermopan panning is pre-cut to standard sizes to fit common floor joist and stud cavity dimensions.
What other products does Thermo Manufacturing make besides ThermoPan?
The company also makes headers, saddles, connectors, hanging hardware, tapes, sealants, grilles, registers, diffusers, levelers, and frames for return air duct systems.
Is Thermopan made from sheet metal?
No, Thermopan is a corrugated material faced with aluminum, built as an alternative to sheet metal ductwork.