Luxairy Vents makes flush-mount air vent covers designed to blend into a wall or ceiling rather than stand out as a visible grille. The line covers permanent cold air return vents, removable air supply vents, access panel covers, exhaust fan covers, and filter clips, sold as separate series aimed at each application.
The brand's covers are made to be paintable or wallpapered over so a contractor or homeowner can finish them to match the surrounding surface. This is the core selling point across the product line.
Product Lines
The PermaFlow series covers permanent cold air return vents in flush-mount sizes from 8 inches to 24 inches. The Breezelux series covers removable air supply vents in 3-inch to 6-inch widths. The AccessPro series covers access panels from 6-inch to 20-inch openings, and the SilhouEase series covers exhaust fans.
The CliqueElite series covers cold air returns, and Luxairy also sells filter clips as an accessory across its return vent lines. Surfaces on these covers are built to be paint-ready or wallpaper-friendly so the finished vent can be customized to match the wall or ceiling around it.
Why Contractors Specify Luxairy Vents
On remodel and finish work, a visible metal grille can be the one detail that breaks an otherwise clean wall or ceiling. Luxairy's flush-mount design and paintable surface let a vent cover disappear into the surrounding finish instead of standing out as hardware. This matters most on higher-end residential jobs where the client is paying close attention to sightlines.
The covers come in a range of sizes across return, supply, access panel, and exhaust fan applications. A contractor can usually source multiple vent types from one line for a single job rather than mixing brands room to room.
How to Choose Luxairy Vents Products
Match the series to the application first: PermaFlow for permanent cold air returns, Breezelux for removable supply vents, AccessPro for access panels, and SilhouEase for exhaust fan covers. Each series runs its own size range, so confirm the opening dimensions on site before ordering.
Decide on finish treatment before installation, since these covers are meant to be painted or wallpapered to match the wall or ceiling. Plan that finishing step into the job schedule rather than treating it as an afterthought, since an unfinished cover will stand out more than a traditional grille would.
Frequently Asked Questions
What makes Luxairy Vents different from a standard metal grille?
The covers are flush-mount and designed to be painted or wallpapered to match the surrounding wall or ceiling, rather than staying visible as a separate piece of hardware.
What sizes does the PermaFlow series come in?
PermaFlow covers permanent cold air return vents in flush-mount sizes ranging from 8 inches to 24 inches.
Can Luxairy vent covers be painted?
Yes. The surfaces are built to be paint-ready or wallpaper-friendly so the cover can be finished to match the room around it.
Does Luxairy make covers for exhaust fans and access panels, not just return and supply vents?
Yes. The SilhouEase series covers exhaust fans and the AccessPro series covers access panels from 6-inch to 20-inch openings, alongside the return and supply vent lines.
What size range does the Breezelux series cover?
Breezelux covers removable air supply vents in widths from 3 inches to 6 inches.