Cherne Industries was founded in 1953, when the company pioneered an inflatable device for stack testing that helped establish the modern pneumatic test plug. Oatey acquired Cherne in 1990, and the brand now operates as part of the Oatey Family of Companies.
Cherne makes both pneumatic and mechanical test plugs from 100 percent natural rubber, without chemical fillers or resins, aiming for reliable sealing across plumbing and waterworks testing applications.
Product Lines
SupplyHouse carries Cherne's plumbing test plugs, sized six inches and smaller, alongside the brand's waterworks plugs built for larger pipe diameters of eight inches and up. The lineup includes pneumatic Test-Ball plugs, mechanical cleanout plugs, and the robotically manufactured I-Series test plugs, which extend up to sixty inches for large-diameter waterworks testing.
Cherne also supplies testing equipment for manhole, smoke, joint, and hydrostatic testing, along with gauges and accessories that support the plugs during a test.
Why Contractors Specify Cherne
Contractors specify Cherne because the brand has built test plugs since 1953. It positions itself as a leader in pipe plug and testing equipment across both plumbing and waterworks trades. Manufacturing plugs from 100 percent natural rubber without chemical fillers gives Cherne products a sealing reliability. Contractors rely on that reliability for pressure and leak testing before a system goes into service.
Cherne covers both small plumbing diameters and large waterworks pipe with the I-Series line. Crews doing municipal or commercial testing work can standardize on one plug brand instead of switching suppliers based on pipe size.
How to Choose Cherne Products
Choosing the right Cherne plug starts with measuring the exact pipe diameter being tested, since plumbing plugs and waterworks plugs are built for different diameter ranges and pressure requirements. Contractors should decide between pneumatic and mechanical plugs based on the test method required by the job or local code, since each type seats and releases differently.
For large-diameter waterworks testing, the I-Series line covers pipe up to sixty inches. Confirming the plug size matches the pipe before scheduling a test avoids a delay on site. Checking the plug's rated test pressure against the system's actual test requirement is also necessary before starting a hydrostatic or pneumatic test.
Frequently Asked Questions
How long has Cherne been making test plugs?
Cherne Industries was founded in 1953 and pioneered an inflatable device for stack testing. The company has continued developing pneumatic and mechanical test plugs since then.
Is Cherne owned by Oatey?
Oatey acquired Cherne in 1990, and Cherne now operates as part of the Oatey Family of Companies. Cherne continues to manufacture test plugs and testing equipment under its own brand name.
What material are Cherne test plugs made from?
Cherne manufactures its pneumatic and mechanical test plugs from 100 percent natural rubber, without chemical fillers or resins. The material choice is intended to support reliable sealing during pressure and leak testing.
What is the difference between Cherne's plumbing and waterworks plugs?
Cherne's plumbing plugs are sized for pipe six inches and smaller, while its waterworks plugs cover eight inches and larger. Choosing between them starts with measuring the exact pipe diameter being tested.
What is the I-Series test plug?
The I-Series is Cherne's robotically manufactured test plug line. It extends up to sixty inches, covering large-diameter waterworks testing applications.