Saniflo is the United States brand of SFA Group, a French manufacturer that developed one of the first macerating toilet systems in 1958. SFA originally designed water treatment plant equipment before adapting macerator technology for residential and commercial plumbing. This allowed toilets, sinks, and other fixtures to be installed above the floor without cutting into existing drain lines. Group SFA expanded into Canada in the late 1980s and established Saniflo as its United States subsidiary in 1998. Today Saniflo serves plumbing contractors and homeowners working on renovations, basement finishes, and additions where running new below-floor drainage is not practical.
Product Lines
Saniflo's core product line is the macerating pump. It grinds waste and toilet paper into a slurry before pumping it up and out to a soil stack or municipal sewer connection. This lets a full bathroom go in almost anywhere in a building. The Saniplus and Sanigrind families cover full-bathroom installations, while smaller units are built for a single toilet or a half-bath addition. Saniflo also manufactures grey water pumps for sinks, showers, and washing machines. It also makes lifting stations sized for basement and commercial applications that need to move multiple fixtures' wastewater to a single discharge point. Each product line is built around the same core macerating or grinding mechanism, sized differently for the fixture load it serves.
Why Contractors Specify Saniflo
Contractors reach for Saniflo when a project calls for adding plumbing fixtures below a home's existing drain line or far from the main soil stack. A macerating system removes the need to break up a slab or reroute gravity drainage. That makes basement bathroom additions, in-law suites, and older buildings with awkward drain layouts practical jobs instead of major excavation projects. Saniflo's parent company developed one of the first macerating toilet systems in 1958. Contractors can specify a system with a long track record rather than a newer, unproven alternative. The above-floor installation method also shortens labor time on the job compared to trenching a new drain line.
How to Choose Saniflo Products
Choosing the right Saniflo unit starts with counting the fixtures it needs to serve. A single toilet needs a smaller macerator than a full bathroom with a toilet, sink, and shower or tub feeding the same unit. Distance and vertical lift matter next, since each Saniflo model is rated for a maximum horizontal run and vertical discharge height that the installation cannot exceed. Grey-water-only fixtures, such as a standalone sink or washing machine, call for a grey water pump rather than a full macerating unit built to handle solid waste. For basement or commercial applications serving several fixtures at once, a lifting station sized for that combined flow is the more appropriate choice than a single-fixture macerator.
Frequently Asked Questions
What does a Saniflo macerating pump do?
A Saniflo macerating pump grinds toilet waste and paper into a slurry. It then pumps the slurry up and out to a soil stack or sewer line. This lets a bathroom be installed without a below-floor drain connection.
Can Saniflo units handle a full bathroom?
Saniflo's Saniplus and Sanigrind families are built for full-bathroom use, handling a toilet along with a connected sink, shower, or tub on the same unit.
Is a Saniflo system different from a sump pump?
A Saniflo macerating pump grinds and pumps waste from a toilet or other fixture, while a standard sump pump moves clear or grey water only. Saniflo's grey water pumps serve sinks and washing machines separately from its toilet-rated macerators.
What limits should I plan around when installing a Saniflo pump?
Each Saniflo model is rated for a maximum horizontal run and vertical discharge height. The installation cannot exceed either rating.
Who manufactures Saniflo products?
Saniflo is the United States subsidiary of Group SFA, a French manufacturer that developed one of the first macerating toilet systems in 1958.